=======================
ProPxD Version 2.1.1
=======================


*********************************************************
IMPORTANT - PLEASE READ BEFORE STARTING THE INSTALLATION
*********************************************************


*********************************
How to install ProPxD V2 (2024):
*********************************

1. Please check if you already have "ProPxD V2 (202x)" installed on your system. 
   If the installed version is LOWER than 2.0.3, please uninstall "ProPxD V2 (202x)" manually via the Windows Control Panel.
  
   (Note: All versions of ProPxD V1 (ProPxD Communication Software) can remain on your system)

2. After deinstallation, make sure that the ProPxD program installation folder (for example: C:\Program Files\ProPxD) is empty.
   If this is not the case, delete the entire contents of the "ProPxD" folder manually.

3. Unzip the installation files and then launch "setup.exe".

4. Follow the instructions of the installation tool for ProPxD V2 (2024) version 2.1.1.